This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Z-Stack Home SmartRF05EBCC2530

Other Parts Discussed in Thread: Z-STACK, CC2530, CC2652R

I need information about developing a battery powered tubular motor with Zigbee embedded with the motor. I saw on the Zigbee Alliance website that TI has the Z Stack product that connects via Zigbee. I was the motor to be able to communicate with the Amazon Echo Plus via the zigbee in the motor.

Z-Stack Home SmartRF05EBCC2530 

  • For CC2530, you can use Z-Stack 3.0.2 and SampleLight example is a good start point for you to implement tubular motor controller. By the way, CC2530 is a old chip for Zigbee application. If it is a new design, I would suggest you to use CC2652R instead of CC2530. For CC2652R running Zigbee Stack, it’s much more resourceful and you can refer to Simplelink Academy at to learn more about how to use CC2652R to run Zigbee Stack and you can fined related examples at