This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531: Unable to flash CC2531

Part Number: CC2531


Hi, last couple of hours I'm trying to flash my CC2531 but the CC Debuger LED is still red. When the CC2531 is connected to the PC the LED on the stick is green but as soon as I connect it to the adapter between CC Debugger and the stick, the LED on the stick turns off. Also the LED on the CC Debugger flashes green when I connect it to the PC (no matter if it's connected to the CC2531) but then immediately changes to red and stays this way. Is the adapter broken? I already run out of answers on the web.All of my components are from AliExpress.

I'll answer common questions right away:- I have tried in on two different PCs, one with Linux, one with Windows- I have tried to reverse and other combinations with the cable going from adapter to the stick- I have updated the CC Debuger firmware (05CC 0044)- Both stick and debugger are in the USB ports- Tried using the reset button on both debugger and the stick with various cable combinations- When stick and debugger are not connected together, PC detects them both. When I connect them the stick is lost- The debugger does have the green led too, because it flashes for short period of time

Please help me I'm desperate. I have been waiting for the package 11 weeks and now it doesn't work