This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: What is difference between CC152P-1, CC152P-2 & CC152P-4 LaunchPad?

Part Number: CC1352P

Hello Community,

I would like to know the difference between CC152P-1, CC152P-2 & CC152P-4 LaunchPad.

Will you please help me know more about these products?

Regards,

Shiv Patil.

  • LAUNCHXL-CC1352P1:

    • Sub-1 GHz operation at 868 MHz / 915 MHz up to +20 dBm
    • 2.4 GHz operation up to +5 dBm

    LAUNCHXL-CC1352P-2:

    • Sub-1 GHz operation at 868 MHz / 915 MHz up to +14 dBm
    • 2.4 GHz operation up to +20 dBm*

    The new P-4 design will support: 433 MHz up to 14 dBm and 2.4 GHz up to 10 dBm (the 20 dBm PA will be HW-optimised for 10 dBm operation).