Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK,
Hello,
I have been working on an application code base on the sampleLight example from Z-Stack Home 1.2.2a.44539. At first I tried putting my ZED to sleep by enabling the POWER SAVING flag in the compiler option but that never seemed to put the device to sleep. So I decided to do it on my own. I set an event to make the device sleep every 30 seconds for 1 minute (the durations used are for testing purposes) and the code is like this. My problem is that the reports to the router are often not send and I am not sure why. The reports are set to fire up every 60 seconds. What could be the issue for it ? Am I omitting something ?
if(events & MEAZON_MISC_WATER_SLEEP_TIMEOUT_EVT)
{
if ( MAC_PwrOffReq(MAC_PWR_SLEEP_DEEP) == MAC_SUCCESS )
{
ui32Val = SleepModeTimerCountGet();
SleepModeTimerCompareSet(ui32Val + 274285);
HAL_TURN_OFF_NWK_LED();
SysCtrlDeepSleep();
/* Update the osal timers and clock with the sleep time */
osalAdjustTimer(60000);
MAC_PwrOnReq();
}
osal_start_timerEx( meazonMiscTaskID, MEAZON_MISC_WATER_SLEEP_TIMEOUT_EVT, 30000 );
return ( events ^ MEAZON_MISC_WATER_SLEEP_TIMEOUT_EVT );
}
Thank you for your time
Nomikos Panagiotis