Other Parts Discussed in Thread: CC2530EM, Z-STACK, CC2530
Hi,
I wonder if anybody else has seen this issue? I was experimenting with Zigbee networks using 2 SmartRF0EB and some CC2530EM modules. All is well, I can program the light_switch.hex, spectrum_analyzer.hex and per_test.hex examples and they work fine out-of-the-box.
I compiled Z-Stack 3.0 GenericApp and programmed it on the SmartRF05EB/CC2530EM to set up Coordinator, Routers and End Device. This works on one SmartRF05EB/CC2530EM set but when I move the CC2530EM to another SmartRF05EB then it seems to power cycle (The LCD shows: Texas Instruments ... SW4: Help, which flashes on and off as if it is power cycling, LED2 also blips). This pointed to perhaps a hardware fault on one of my SmartRF05EB boards (However, probing the power lines, they all seem stable). Also that particular board works with the previous demos. I looked at the Joystick pin voltages and they don't seem to be faulty or stuck with a particular output.
This pointed to perhaps some issue with the GenericApp code rather than a hardware fault on the SmartRF05EB board. Batteries have been changed to new ones, that didn't seem to be the issue.
Has anybody else seen this behaviour ? Out of interest what is the Joystick part number on the SmartRF05EB, I think I'll swap it for a new one.
Regards,
Ian