Other Parts Discussed in Thread: CC2591
Hello,
I'm studying the wideband of a coordinator and an end device while they are sending messages between themselves every 5 seconds.
They are in the same network and supposedly in the same channel.
The problem is that I detect peaks in all the channels after the network is created and the spectrum analyzer is only connected to the coordinator in one case and to the end device in the other case.
This are the photos of the two cases:
This one is result of the coordinator, it is working with a cc2591 as a front end.

This one is from the end device: