Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
Hi,
I'm new to ZigBee and TI programming, used to program Arduino. I red many of the articles but not sure I understand the ZAP and ZNP.
First I would like to upload the blinking LED code to CC2530. I downloaded the code from this forum, which seems all right but for whatever reason it doesn't blink the LED.
If I understand correctly the steps are as follows:
1; create a HEX file from the BINKIG LED code (I used KEIL)
2; using cc debugger and Smart RF Flash programmer ( version 1) upload the HEX file.
My questions:
1; Is this the right way to do it, or did I miss something?
2; Can i use cc2530 on its own as a microcontroller as well as a ZigBee device, or do I need a separate microcontroller for it?
Many thanks for your help
Daniel