This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538: Unable to test the RF signal strength using CC2538 & the Smart RF Studio 7

Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK, CC1352R, CC1352P, CC2592, , , SMARTRFTM-STUDIO, CC2652P

Hello Community,

I am working on the CC2538 Zigbee device with the SmartRF06 Evolution Board.

I am trying to test the transmission & reception power between the 2 CC2538 devices using the Smart RF Studio 7.

I referring the following document, 

https://www.ti.com/lit/ug/swru194b/swru194b.pdf?ts=1595397320175&ref_url=https%253A%252F%252Fwww.google.com%252F

I have done the following steps,

1. Connected CC2538 module to the SmartRF06 Evolution Board.
2. Connected the SmartRF06 Evolution Board to the PC.
3. Verified the evolution board drivers are installed.
4. Flash both the CC2538 module with the ZNP firmware application.
5. Started smart RF Studio 7.
6. opened the configuration window of the connected devices.
7. Selected easy mode. Assigned one RF board as Tx & other as Rx.
8. Set the same freq, channel & power settings. Also the selected beacon packet on both sides.
9. Started the transmission & reception.

But, 
I am unable to get the packet on the Rx side of the Smart RF Studio 7.
Is there anything wrong I am doing?


Will you please help me to know how can I test the RF strength for the CC2538 devices.

Regards,
Shiv Patil.