Other Parts Discussed in Thread: Z-STACK
I need a simple modification to znp firmware.
I need to have in the CC1352 + znp firmware a string and I need a MT command for request the custom string.
My cuestion,
1 -) Can I use a MT command defined in the standar Z-Stack Monitor and Test API?
if yes
1.1-) which MT command?
if no
1.2-) Can I use a custom MT command?
if yes:
1.2.1-) What should be the values of the fields: type, subsytem and ID in the custom MT command?
1.3-) I which znp firmware section I must to ask by the incomming MT command?
Thank you very much!
Best Regards!