This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: CC2530: Group cast in ZSTACK3.0.2 & Z-Tool . Buf the delivery mode isn't GroupAddressing

Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK

Hello

I use the Zstack-3.0.2 and Z-Tool to test group cast.

First, I use the ZDO_EXT_ADD_GROUP to call aps_AddGroup() .

Secondlly, I use the AF_DATA_REQUEST to add two routers to the group, the response is successful.

Finally,I use the AF_DATA_REQUEST_EXT to send group cast to routers. Routers can control.

But in packet sniffer, the Delivery Mode in APS Header is Broadcast. Why not is Group Addressing?

This is screenshot of Z-Tool.

This is screenshot of the packet sniffer.