Part Number: CC1352P
Other Parts Discussed in Thread: SIMPLELINK-CC13X2-26X2-SDK, TIDC-ZNP-HOST-SW3, Z-STACK, CC2538, , CC2592
Hello Community,
I am working on ZNP host Framework Application with CC1352P-2 ZNP device.
I am using the ZDO_MGMT_PERMIT_JOIN_REQ with following configurations.
root@testdevice:/home/test/znp-host-framework/examples/cmdLine/build/gnu# ./cmdLine.bin /dev/serial/by-path/platform-3f980000.usb-usb-0:1.3:1.0 Do you wish to start/join a new network? (y/n) n Resetting ZNP EndPoint: 1 Network Error mtSysGetExtAddrSrspCb ExtAddr: 0x00124B001CA609BA Enter CMD ZDO_MGMT_PERMIT_JOIN_REQ Command: ZDO_MGMT_PERMIT_JOIN_REQ Enter AddrMode: (1B) 0x02 Enter DstAddr: (2B) 0x0000 Enter Duration: (1B) 0x3C Enter TCSignificance: (1B) 0x01 mtZdoMgmtPermitJoinRspCb SrcAddr: 0x0000 Status: 0x00
SOC OUT --> LEN :05, SOF :FE, CMD0 :25, CMD1 :36, Payload :02:00:00:3C:01, FCS :29
SOC IN <-- LEN :01, SOF :FE, CMD0 :65, CMD1 :36, Payload :00, FCS :52
SOC IN <-- LEN :03, SOF :FE, CMD0 :45, CMD1 :B6, Payload :00:00:00, FCS :F0
After that I am getting ZDO_TC_DEV_IND.
SOC IN <-- LEN :0C, SOF :FE, CMD0 :45, CMD1 :CA, Payload :84:0F:XX:XX:XX:XX:00:4B:12:00:00:00, FCS :6D
mtZdoTCDevIndCb :
SrcNwkAddr: 0x0F84
ParentNwkAddr: 0x0000
IEEEAddr: 0x00124B00XXXXXXX
Problem with this is,
The device is get removed after few seconds when ZDO_TC_DEV_IND callback hits.
Will you please help me to know why this is happening???
Am I missing someting after getting ZDO_TC_DEV_IND. (i.e providing link key to device OR other permit joining related configurations)
please refer sniffer logs give below.
Regards,
Shiv Patil.