Part Number: CC2530
Other Parts Discussed in Thread: CC-DEBUGGER, CC2531EMK, CC2531
Hi,
the last days I tried to flash my CC2530 but couldn't get the TI CC Debugger to recognize the chip.
The connections are the following:
Debugger -> Chip
GND -> GNDs
Target Voltage Sense -> VCCs
DD -> P2.1
DC -> P2.2
RESET -> RESET
3.3V -> VCCs
I also measured the ribbon cable through and there should be no problem. The USB cable should be fine as well, as the CC Debugger is getting recognized just fine by the PC.
Currently I have no components other than the debug-connector attached to the chip. Are other components essential to connect so I can flash the chip succesfully (e.g. external RF-clock)?
Best regards,
Dieter