Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
Tool/software: TI C/C++ Compiler
Hi Team,
1.There is "-DZDNWKMGR_MIN_TRANSMISSIONS=20" In f8wConfig.cfg.
/* Minimum transmissions attempted for Channel Interference detection, * Frequency Agility can be disabled by setting this parameter to zero. */ -DZDNWKMGR_MIN_TRANSMISSIONS=20
As explained above, if this parameter is set to 0, frequency agility can be turned off.
However, in the nwk_globals.h file:
// The PANID Conflict feature is mandatory for both 2007 and 2007 PRO. // So, it will be ON all the time (except sleeping end devices). #if !defined (ZIGBEE_PANID_CONFLICT) #define ZIGBEE_PANID_CONFLICT
So, if setting " -DZDNWKMGR_MIN_TRANSMISSIONS=0 ", is the frequency agility turned off completely?
2.If the frequency agility is set to "-DZDNWKMGR_MIN_TRANSMISSIONS=0" and it is closed, so the change of this channel is initiated by the coordinator、 router node or end divice ?
(1) If it is initiated by the coordinator,when I want to turn off frequency agility,Just turn off the frequency agility setting in the coordinator project ( -DZDNWKMGR_MIN_TRANSMISSIONS 0)
and other nodes setting to -DZDNWKMGR_MIN_TRANSMISSIONS 20 or 0 . Is this statement correct?
(2) If all nodes can evaluate the channel interference environment, then this parameter must be unified and the same.
Which one is correct between (1) and (2)?
Regards,
Kevin