Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: UNIFLASH
Short description: LAUNCHXL-CC26X2R1 Defective board (Case No.: CS0293727)
I got two boards of LAUNCHXL-CC26X2R1 and one of them is dead.
I had open first box and try to flash it, but uniflash is not able to detect it. I had open second one, and it has no problem.
Both has two leds on XDS110: red and green. On the first (defective) board, only the red LED was lit on the second the green.
xdsdfu is not able detect first board.