Part Number: CC1352P
Other Parts Discussed in Thread: Z-STACK
Hello community,
We are working on a Zigbee project with a CC1352P connected to an AM437x. We currently have a problem with the LEAVE. To remove devices from the network, we use the NWK_REMOVE_DEVICE_REQ command as described in the documentation and as it is implemented in the example application made in NodeJS. This command returns a NWK_ZIGBEE_DEVICE_IND_VALUE with nwkDeviceStatus_t.DEVICE_REMOVED, and when we check the server's CSV files, the device is deleted (commented line). However, when we check Ubiqua we see that the LEAVE command was not sent to the device. We have devices that behave in a specific way when they are removed from the network (for example, they show "no net"), and we see that this does not happen. We have tested with different types of devices and always nothing. What could be the problem here and how can we fix it ???
BR,
Randy