Other Parts Discussed in Thread: Z-STACK, SYSCONFIG
Hi!
I encountered a problem when using the DMM (Zbee + Ble) stack. Right now I am using a modified dmm example, running v4.20.1.04 stack and TI 20.2.1LTS compiler.
I managed to write some data to the Flash using the osal_snv_write, it works reliably, but whenever the zigbee stack is starting commision then the memory fails at write (the read still works)
The osal_snv_write returns a non-standard value EG "536923948 ". It does not matter if the Zbee is in commisioning mode or not or I restart the board.
The only fix is to erase the flash and reprogram the board, then it works until I start Zbee commisioning.
Do you have any suggestions?
Thank you!