Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK
I"m using z-stack 3.0.2, and I'm using zigbee for RSSI location. The msg which I broadcast is send to all neighborhood devices, which if is routers, it will re-sent the msg to the coordinator with the collected RSSI.
I'm using this command lines in End Device:
dstAddr.addr.shortAddr = NWK_BROADCAST_SHORTADDR_DEVZCZR;
dstAddr.addrMode = (afAddrMode_t)AddrBroadcast;
dstAddr.endPoint = AF_BROADCAST_ENDPOINT;
status = AF_DataRequest(&dstAddr, &NanoTrack_EpDesc, ZCL_CLUSTER_ID_NANOTRACK,
Z_EXTADDR_LEN, &buffer[0], &NanoTrack_TransID, AF_DISCV_ROUTE | AF_SKIP_ROUTING, 1);
But, using this command, the msg is only delivered to my EndDevice parent.
Is there something that I'm missing?
Does MULTICAST_ENABLED=FALSE play a role on this? Or there is another #define that I must use to achieve this?
Thanks!