Part Number: CC2538
Other Parts Discussed in Thread: SMARTRF06EBK, Z-STACK
Hello,
I would like to ask a question concering the power saving mode in CC2538. I am using the zstack 1.2.2a HomeAutomation. The device is falling asleep and it wakes up with the sleep timer interrupt. i would like to set a GPIO interrupt as well and I want to register an interrupt service routine for that GPIO when it wakes up. The sleep wake up timer has a dedicated interrupt service routine to set does the GPIO has one also or do I use the generic function to set a GPIO interrupt?
Thank you in advance
Panagiotis Nomikos