Part Number: CC2530
Other Parts Discussed in Thread: CC-DEBUGGER, TPS65910
Given the issues I have to reset the CC2530 from the software running on the AM335x based platform, I checked the analog value of the reset. I had the impression that I needed to do a power cycle to reset the CC2530, but I've tried enough times to reset the ZNP by conrolling the reset from SW without success followed by a power cycle that succeeded, that I am now pretty close to certain that there is an issue with the RESET_N input signal:

As far as I understand from the specification, when powered at 3.3V, the logic input level must be minimum 2.5V for all digital inputs in order to have a valid HIGH value. As at the same time the CC2530 only guarantees an output of 2.4V@4mA, I wanted to double check this with a TI Expert. I may have overlooked a comment specific to the reset level.

What is the minimum reset level? Is the reset signal shown above ok?