Part Number: CC2652P
Other Parts Discussed in Thread: SIMPLELINK-CC13X2-26X2-SDK, Z-STACK, Z-STACK-ARCHIVE, CC1352R, CC2652R, CC1352P, SMARTRFTM-STUDIO
Hi ,
I am planning to build a gateway using CC2652P ZigBee chipset.I would like to know the below details regarding CC2652P ZigBee chipset.
1.Does it have ZigBee Alliance certification ?
2.Deos it have support for DotDot ?
3.Does it have support for ZigBee 3.0 (ZigBee 2006 / ZigBee Pro 2015) ?
4.Does it support latest ZigBee HA profile ? what is the version supported ?
5.Does it support latest ZigBee Smart Energy profile ? what is the version supported ?
6.Does it support a maximum of 100mW (20dBm) EIRP ?
7.The product will support ~15m range, including penetration of 3 walls (indoor and outdoor) equivilant to brick density (RSSI -70dB). Note: Attenuation of 3 to 4dB internal (dry wall), 6 (single course) to 18dB (double course cavity). Is it possible with the module?
8.Will it have any impact on existing deployment of other 2.4GHz interfaces on the gateway ?
The above answers will help to decide on the chipset selection. Please provide info on the above.
Thanks,
Vikas