Part Number: CC1352P
Other Parts Discussed in Thread: Z-STACK
Hello community,
We are working on an application to control Zigbee, using a CC1352 as a coordinator.
We have a Zigbee device to connect it to the coordinator, which during its initial configuration sends 2 messages that are automatically answered by the coordinator. Reply messages are different than they should be. Although these messages are sent automatically by the coordinator, we decided to forward them correctly to see if the end device takes the data it needs and is configured correctly. However, whenever we try to send these messages from the application, the coordinator or Linux server returns "Failure" and the message is not sent to the device.
Our doubts are:
-Can we deactivate these automatic response messages in any way and control them from the application, to ensure that they are sent correctly?
-Deactivating this, will allow us to send those messages and will not return "Failure"?
So that I can explain myself better, I leave you images of the messages
1- Read Attribute Response
Our environment
Original environment
2- Default Response
Our environment
Original environment
Best Regards,
Randy