Other Parts Discussed in Thread: SIMPLELINK-CC13X2-26X2-SDK
Hi,
I just bought a LAUNCHXL-CC26X2R1 board and want to pair to my Zigbee coordinator (CC2652RB development stick) with zigbee2mqtt firmware. I uploaded successfully "zed_sw" and "zed_light" demos to the board, but when I press the BTN-1 the searching process starts and counting from 180 to 0 and no pair success. Other zigbee devices like SONOFF SNZB-02 works perfectly.
Any idea? What am I doing wrong? Thanks!
Board uart status:
Device Info: [IEEE Addr] 00124B00219FB207 [Power Mode] Sleepy
NWK Info: [PAN ID] 0x1a62 [Channel] 11 [Short Address] 0x96a0
NWK Info: [Parent Address] 0x0000
ZDO Info: [Logical Device] End Device [State] In the network
BDB Info: -- JOIN Id000 Srch173/00
Bind Info: --
APP Info: [Remote Light] 0xffff state is Unknown
In my coordinator I am getting only:
{
"message": "announce",
"meta": {
"friendly_name": "0x00124b00219fb207"
},
"type": "device_announced"
}
OR