Part Number: CC2530
Hi,
I am using CC2530 as ZCD, Now I want to change the Pan ID for ZCD.
1) Which command should I use to change PAN ID in Z-tool.
Thanks & Regards
Pavithran J
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2530
Hi,
I am using CC2530 as ZCD, Now I want to change the Pan ID for ZCD.
1) Which command should I use to change PAN ID in Z-tool.
Thanks & Regards
Pavithran J
Hi Pavithran,
I assume you are speaking of a ZNP set as a ZC node role. You can follow YK's blog post to set up a Zigbee 3.0 network with SYS_OSAL_NV_WRITE to set the ZCD_NV_PANID (0x0083). You can alternatively use UTIL_SET_PANID. This must be done before commissioning the network, otherwise a factory reset must be performed to erase the NV memory. Please refer to the Monitor and Test API for more information.
Regards,
Ryan