Part Number: CC2652P
Other Parts Discussed in Thread: CC2592
Hello,
I am trying to read chip id from external flash winbond W25X40CL from master CC2592 in my application.
Followed SPI master example and flash datasheet for instruction set. I have integrated sample code in my application to read/write data on external flash.
I am getting 0 in response of get chip id (0x90) command. How can I read read/write data successful?
Please, find the code snippet below.
SPI_Handle masterSpi;
SPI_Params spiParams;
SPI_Transaction transaction;
bool transferOK;
/* Open SPI as master (default) */
SPI_init();
GPIO_setConfig(CONFIG_GPIO_1, 1);
SPI_Params_init(&spiParams);
spiParams.frameFormat = SPI_POL0_PHA1;
spiParams.bitRate = 4000000;
spiParams.mode = SPI_MASTER;
masterSpi = SPI_open(CONFIG_SPI_0, &spiParams);
if (masterSpi == NULL) {
debug_uart_write_str("Error initializing master SPI\n");
while (1);
}
else {
debug_uart_write_str("Master SPI initialized\n");
}
masterTxBuffer[0] = 0x90;
masterTxBuffer[1] = 0x00;
masterTxBuffer[2] = 0x00;
masterTxBuffer[3] = 0x00;
transaction.count = 4;
transaction.txBuf = (void *) masterTxBuffer;
transaction.rxBuf = (void *) masterRxBuffer;
GPIO_write(CONFIG_GPIO_1, 0);
/* Perform SPI transfer */
transferOK = SPI_transfer(masterSpi, &transaction);
if (transferOK) {
debug_uart_write_str("SPI status = %d\n", transaction.status);
if(transaction.rxBuf != NULL)
debug_uart_write_str("Master received: %02x\n", masterRxBuffer[0]);
else
debug_uart_write_str("RX buff is NULL\n");
}
else {
debug_uart_write_str("Unsuccessful master SPI transfer");
}
GPIO_write(CONFIG_GPIO_1, 1);
Regards,
Ankit S