This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: ZTool won't detect it

Genius 9880 points
Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK

Hi Team, 

Customer having problem with their CC2530 working as a Zigbee Network Processor. Below is the inquiry.

"
My goal is to design a Zigbee end device. I've decided to use the CC2530 since it seemed to be the best solution for my needs (low cost + low power)

What I did so far is :
• Download Zstack 3.0.2
• Build the ZNP project (Z-Stack 3.0.2 > Projects > zstack > ZNP > CC253x) with IAR Workbench IDE - 8051 10.30.1)
• Upload the firmware to the CC2530 using the CC Debugger with Flash Programmer v1 (www.ti.com/.../FLASH-PROGRAMMER)
• Upload is successful

What doesn't work :
• Ztool won't recognize the CC2530.

The CC2530 is plugged with a FTDI USB => UART converter. I plugged everything according to documentation

CC2530 FTDI USB => UART
P1_4 (CT) RTS
P1_5 (RT) CTS
P1_6 (TX) RX
P1_7 (RX) TX
P1_2 (CFG0) GND
P2_0 (CFG0) GND
"
Regards,

Maynard