Hello, I have used Z-Stack Linux GW with Raspberry Pi 3 so far without any problem. Now I want to use Raspberry Pi zero W but when I run Z-Stack Linux application it issues "Illegal instruction" errors. When I searched for it I found this post and the same problem, so I changed the -march flags from armv7-a to armv6 and recompiled Z-Stack Linux GW. But unfortunately the problem still exists! Is the any other thing that I must do in order o run Z-Stack Linux GW on Raspberry Pi zero w?
Regards, Ahmad.