This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Output Power

Other Parts Discussed in Thread: CC2530, CC2531, CC2591

Hello,

I am writing to  ask about the features to change the  output power.

I am working with cc2530 device and the device is able to programable up to 4.5 dbm. I want the maximum Output Power Up to obtain the maximum distance comunication between the devices.

Can you tell me more things to obtain more distance between the devices? (using the same hardware, only changes the firmware)

Regards,