Part Number: CC2652P
Other Parts Discussed in Thread: SMARTRF06EBK, Z-STACK, SYSCONFIG
Dear All,
I'm beginning a project with CC2652P1FRGZ (bought EByte E72 2G4M20S1E module on internet) (This project is to replace an obsolete Freescale Uart to Zigbee transceiver)
I've experience with 280xxx devives but nothing nothing with CC Rf devices.
1) I've a working XDS100 V2 14 pins interface (at least with 28032 and 280049 devices) but I'm unable to connect and establish link with CC2652P1
Is it possible to use XDS100 V2 with CC2652P1 Devices ?
If yes, I've connected 4 JTAG pins, reset and power, are there other connections on pins configuration to take care ? Is reset necessary ?
2) For Uart to Zigbee interface, which project do you advise me to start with ?
I prefer a project without RTOS.
Thank you by advance
Best regards
francois