Part Number: CC2652R
Other Parts Discussed in Thread: SYSCONFIG
HI,
We are using a sample code from SDK with ZED configuration which already as Standby mode policy defined in the sysconfig. with this default configuration from sample code (SDK) current measured is ~100 uA. which we assume because of below stand by mode config:
Standby without cache retention : RTC running, CPU, 80KB RAM and (partial) register retention, RCOSC_LF -> 0.94 μA.
how to configure device to enter into below mode?
Standby without cache retention : RTC running, CPU, 80KB RAM and (partial) register retention, XOSC_LF -> 1.09 μA
Regards
Nikhil