This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650MODA: Unable to program CC2650MODA module.

Part Number: CC2650MODA

Hi,

We have directly connected MODA to the required connections through wires and tried to program it.

We were able to detect the module in Flash Programmer 2 and also loaded Simple_peripheral Project after making the change

//#define CC2650EM_7ID
#define CC2650EM_5XD

It started advertising but we were unable to connect from any android device.

But suddenly the MODA is not getting detected in Flash Programmer 2 and CCS.

When I try to load the Code from CCS, I get the error:

Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 6.0.579.0)

What might have possibly gone wrong after the first program load? Why are we not able to detect board after flashing the code?

The Module is still advertising with the name SimpleBLEPeripheral.

Thank you,

Bharath