Other Parts Discussed in Thread: CC2591, CC2530, TIMAC
Dear sir/Madam,
We are involved in a new project based on CC2530 + CC2591 hardware.
We are using TI Zstack , Zigbee 2006. Mesh topology
One of the requirements of the project is to have the routers powered by battery.
The energy requirements oblige us to put the routers to sleeping 10 seconds and wake up during 10 ms in order to synchronize packets with mesh neighbors.
Can anybody point me in the good direction to solve it?
Is there any TI partner offering this feature as a licensed software?
Thank you in advance,
Ricard