Part Number: CC3200MODLAUNCHXL
Other Parts Discussed in Thread: CC3200
Hi everyone!
I'm stuck with one issue concerning the email application example code included in the CC3200 SDKs.
I have carefully followed and reviewed all the instructions stated at the documentation and everything seem to be all right.
In fact, if I build and run any other internet applications such as wlan_station or get_time I can confirm that the launch pad boards can easily connect with external internet servers such as ti.com or other.
However, and after correctly configuring the demo_config.h macros with my SMTP server parameters (HOST_NAME, HOST_PORT, USER, USER_RFC, PASS,...) I get a failure message at the end of the procedure, as you can see at the below attached dialog captured from the serial console:
*************************************************
CC3200 Email Application
*************************************************
Command Usage
-------------
01 - Connect to Preconfigured AP
03,<to>,<subject>
- Write Recipient Emailaddress(e.g abc@xyz.com) and Subject
04,<message>
- Write Content of the Email
05 - Send Email
06 - Connect to AP Using Smart Config
Parameters
----------
to - Recipient Email Address (e.g abc@xyz.com)
subject - Subject of the Email
message - Content of Email Message
-------------------------------------------------------------------------
Host Driver Version: 1.0.1.6
Build Version 2.7.0.0.31.1.4.0.1.1.0.3.34
Device is configured in default state
Started SimpleLink Device: STA Mode
Cmd#01
[WLAN EVENT] STA Connected to the AP: ISURKI_WIFI , BSSID: 0:13:49:a0:fc:5d
[NETAPP EVENT] IP acquired by the device
Device has connected to ISURKI_WIFI
Device IP Address is 192.168.1.36
OK
Cmd#
Cmd#03,imutuberria@hotmail.com,prueba
OK
Cmd#
Cmd#04,this is a test from SimpleLink
OK
Cmd#
Cmd#05
Get Host IP succeeded.
Host: cp71.webempresa.eu IP: 37.187.166.203
Connection with Email Server Failed, Check Internet Connection and Retry
Cmd#
Cmd#05
Get Host IP succeeded.
Host: cp71.webempresa.eu IP: 37.187.166.203
Connection with Email Server Failed, Check Internet Connection and Retry
Cmd#
Cmd#
Of course, and as I mentioned before, I can check positively that internet connection is properly active and available.
Any suggestion that can help me in this issue would be very much appreciated.
Best regards,
Iñaki