Part Number: CC3120MOD
Other Parts Discussed in Thread: CC3120,
Hi,
I posted before here: e2e.ti.com/.../690896
The SPI Communication is now working as far as i can see it right with my logic analyzer.
I use the provided functions to set the SSID, password, security type, IP, country code and wlan Mode to AP
But i can not see the SSID with my mobile phone so there must still be a problem.
TI does not release any protocol information for the simplelink devices. But it would be much easier for debugging. Is it possible to get these information?
Is there anything special i have to do?
Maybe i set the sl_start and sl_stop at the wrong positions?
The first i do is sl_start then the complete configuration. After that sl_stop directly followed by sl_start. I check the return value of sl_start at its correctly ROLE_AP
Marvin