This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6446 VLYNQ INTERFACE WITH ANOTHER DM6446 VLYNQ

Other Parts Discussed in Thread: TMS320DM6446

Hi!

I want to interface two boards via VLYNQ interface. Each board contains TMS320DM6446 SOC. Can anyone suggest, if it is possible to interface two dm6446 devices over VLYNQ interface? I would want both devices to interrupt each other and originate data send and receive request.

Regards,

Asim

 

  • ASIM said:

    I want to interface two boards via VLYNQ interface. Each board contains TMS320DM6446 SOC. Can anyone suggest, if it is possible to interface two dm6446 devices over VLYNQ interface? I would want both devices to interrupt each other and originate data send and receive request.

    I would say yes, it is possible to connect 2 TMS320DM6446 device via their VLYNQ interfaces.  VLYNQ support bidirectional, peer to peer communication.  I'm not aware of any software implemented that actually does this, but the features of the VLYNQ interface do allow for this capability.

    One caution, VLYNQ is intended for device to device communication on a single PCB with very little loading and relatively short trace lengths.  It is not meant for board to board communication, or cabling, etc.

  • Hi.

    I want to communicate via VLYNQ on two discrete boards.

    Any recommendations on how the interconnects should be? Can I use an external clock (low frequency) to improve signal integrity? Any other recommendations?

  • Yes it is possible to communicate two VLYNQ devices on two different boards.I am able to run the two VLYNQ interface on two different boards using cabling.

     

    Regard's

    RT