Other Parts Discussed in Thread: OMAP3530
I have downloaded DVSDK 3.0 from the following link. http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/dvsdk/DVSDK_3_00/latest/index_FDS.html
BIOS, CSL, xcdtools, OMAP35x-PSP-SDK-02.01.03.11 and CGT tools have the same version as mentioned in Rules.make file. While compiling the DVSDK for OMAP3530 EVM (TI linux using 2.6.22 kernel) the following issues have been seen.
Compiling obj/linux/Cpu.omap3530.o470MV from linux/Cpu.c.. Compiling obj/linux/Display.omap3530.o470MV from linux/Display.c.. Compiling obj/linux/Display_fbdev.omap3530.o470MV from linux/Display_fbdev.c.. linux/Display_fbdev.c:45:29: error: mach/omapfb.h: No such file or directory linux/Display_fbdev.c: In function 'Display_fbdev_create': linux/Display_fbdev.c:260: error: 'OMAPFB_COLOR_YUV422' undeclared (first use in this function) linux/Display_fbdev.c:260: error: (Each undeclared identifier is reported only once linux/Display_fbdev.c:260: error: for each function it appears in.) make[2]: *** [obj/linux/Display_fbdev.omap3530.o470MV] Error 1 make[2]: Leaving directory `/root/dvsdk_3_00_02_44/dmai_2_00_01_04/packages/ti/sdo/dmai' make[1]: *** [all] Error 2 make[1]: Leaving directory `/root/dvsdk_3_00_02_44/dmai_2_00_01_04' make: *** [dmai] Error 2
I added omapfb.h from 2.6.22.18 kernel the following error occured
linux/omap3530/Framecopy_accel.c:51:32: error: linux/omap_resizer.h: No such file or directory linux/omap3530/Framecopy_accel.c: In function 'Framecopy_accel_config': linux/omap3530/Framecopy_accel.c:78: error: variable 'params' has initializer but incomplete type cc1: warnings being treated as errors linux/omap3530/Framecopy_accel.c:79: warning: excess elements in struct initializer linux/omap3530/Framecopy_accel.c:79: warning: (near initialization for 'params') linux/omap3530/Framecopy_accel.c:80: warning: excess elements in struct initializer linux/omap3530/Framecopy_accel.c:80: warning: (near initialization for 'params') linux/omap3530/Framecopy_accel.c:81: warning: excess elements in struct initializer linux/omap3530/Framecopy_accel.c:81: warning: (near initialization for 'params') linux/omap3530/Framecopy_accel.c:82: error: 'RSZ_INTYPE_YCBCR422_16BIT' undeclared (first use in this function) linux/omap3530/Framecopy_accel.c:82: error: (Each undeclared identifier is reported only once linux/omap3530/Framecopy_accel.c:82: error: for each function it appears in.) linux/omap3530/Framecopy_accel.c:82: warning: excess elements in struct initializer linux/omap3530/Framecopy_accel.c:82: warning: (near initialization for 'params') linux/omap3530/Framecopy_accel.c:83: warning: excess elements in struct initializer linux/omap3530/Framecopy_accel.c:83: warning: (near initialization for 'params') linux/omap3530/Framecopy_accel.c:84: warning: excess elements in struct initializer linux/omap3530/Framecopy_accel.c:84: warning: (near initialization for 'params') linux/omap3530/Framecopy_accel.c:85: warning: excess elements in struct initializer linux/omap3530/Framecopy_accel.c:85: warning: (near initialization for 'params') linux/omap3530/Framecopy_accel.c:86: error: 'RSZ_PIX_FMT_UYVY' undeclared (first use in this function)Please help