Hi
In our product we will only have a JTAG connector to the DM355. Is it possible to download montavista along with the uboot through the JTAG. I can not find any document on how to do this.
Any help would be greatly appreciated.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
In our product we will only have a JTAG connector to the DM355. Is it possible to download montavista along with the uboot through the JTAG. I can not find any document on how to do this.
Any help would be greatly appreciated.
Thanks
you can download u-boot thru JTAG, and subsequently load Linux kernel and File System using u-boot. This options is not very well advertised and supported because there is a much simpler and less costly approach (no need to invest in JTAG or IDE) when using the serial boot mode.
http://wiki.davincidsp.com/index.php?title=Serial_Boot_and_Flash_Loading_Utility
However, if you only have a JTAG, then the approach would be similar to that of DM6446. I believe there may be some files present under DVSDK (dvsdk_1_30_00_41/PSP_XX_XX_XXX_XX/bin directory). Unfortunately, I am not in the office to double check this at the moment, but wanted to point you in the right direction. Let us know if you need further assistance.
To confirm Juan's suggestion, there is a dvsdk_1_30_01_41\PSP_01_20_00_014\bin\dm355\NAND_programmer.out which can be used to burn the flash on the DM355, note that this is meant to be loaded by Code Composer Studio as opposed to a third party IDE.