Hi,
The AFE5851 is not supported by the High Speed Data Converters group, but rather is supported by our Medical and High Reliability Group. After this reply, I will try to split this thread and move this portion of the thread to the HiRel forum.
The Medical group supports the TSW1250 Capture Card, which was derived from the TSW1200. Same hardware, but slightly different firmware. The difference is that the TSW1200 does not need to support any data converters that have a frame clock that is 1/2 the sample clock and so the Medical group had to add a modification to the firmware. In the TSW1200, we look for the low-to-high transition of the Frame Clock to indicate where the serial bits of one sample end and the next sample begins. For the AFE5851, the Frame Clock is high for one complete sample and then low for one complete sample. So the firmware had to be modified to look for both the low-to-high locations and the high-to-low transitions of Frame Clock.
So no, the TSW1200 firmware does not support that device without modification. But it should be a relatively easy modification to my source code or the Medical Group can supply their source code.
Regards,
Richard P.