This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5809: AFE5809 Programming question

Part Number: AFE5809


Hello Team,

One of our customers has some misunderstanding in writing coefficient memory block into coefficient RAM on the AFE5809 device. I’ll very appreciate you for some clarification:

Writing decimation filter coefficients to coefficients RAM consist of multiple writes of coefficient memory blocks to SPI address 0xC7. SPI address 0xC7 defined as a 112 bit word which is divided on 8 word of 14 bits each.

Single SPI cycle access of AFE5809 consists of 24 bits which are 8 bit register address and 16 bit data.

So what is the correct way write 112 bit  to 0xC7 register using 24 bit SPI cycle:

  • 8 SPI cycles access to 0xC7 register with SPI data consisting of [15..14] dummy bits and 14 bit [13..0] filter coefficient. ( bits 14 and 15 will be discarded by AFE5809 internal logic)

Or

  • 7 SPI cycle access to 0xC7 register with SPI data consisting of [15..2] coefficient data of one coefficient and two bits [1..0] from the following coefficient  

Thank you in advance!

Kind regards,

Mo.