Hello,
We would like to change the speed of the ICE board to the max. of 720MHz.. I have seen that the therefore the VDD_MPU voltage has to be adjusted to 1.26V. I measure a voltage of 1.08V on the ICE board (TP8). With the GEL file and the script "ARM_TURBO_Config" I can change the clock. How can I change the VDD_MPU voltage?Anyone successfully changed this?How can I change the clock within software (not with GEL script)?
Thanks.
Best regards,Patrick