Hello,
I'm using the AM3354 device with a 8-bit NAND flash, what are the changes I need to make to the U-boot/SPL code. The only define I came across is GPMC_NAND_ECC_LP_x16_LAYOUT, which is defined in the am335x_evm.h file. I have changed it to be x8 instead.
Are there any other changes that I need to make??
Thank you
Regards
Santhosh