This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Linux kernel has a workaround for ARM errata 430973 (Stale prediction on replaced interworking branch)
on a recent DM3730, the workaround must be applied to resolve issues; I want to check against the errata list of the processor -- can you make it available?
which processors are affected by ARM errata 430973?
Processor : ARMv7 Processor rev 2 (v7l)
BogoMIPS : 313.29
Features : swp half thumb fastmult vfp edsp thumbee neon vfpv3 tls
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x3
CPU part : 0xc08
CPU revision : 2
Please refer to following discussion:
http://e2e.ti.com/support/dsp/omap_applications_processors/f/447/t/221514.aspx
Kind Regards,
Maciej Kucia
Peter, you will have to get the full errata directly from ARM. I can tell you that the DM3730 uses the r3p2 version of the ARM core, in which errata 430973 has been fixed, so you should not need to implement the workaround.
Regards,
James
Hello,
I have been told by ARM support that I should get the document from TI;
TI so far pointed me to a document called "ARM Core Cortex-A8 (AT400/AT401) errata" that is available via local FAE
the document "DM3730, DM3725 Digital Media Processors
Silicon Errata (Revs 1.2, 1.1 & 1.0) (Rev. E)", advisory 1.10 (page 39), points to a separate document from TI
I am aware that the DM3730 uses r3p2 of the ARM core and reportedly the errata should have been addressed (but I want to check the errata document)
I am seeing very reproducible segfaults/illegal instruction on a DM3730 when the code for the errata workaround is NOT applied; i.e. I strongly believe that the DM3730 has an issue related to errata 430973
the code in question is public, see http://ssvb.github.com/2012/04/10/cpuburn-arm-cortex-a9.html and try ssvb-cpuburn-a8.S concurrently with other processes; the code is stable with errata 430973 applied in the kernel, but crashes frequently without the errate code applied
thanks, p.
Peter, i think you have the right doc from ARM concerning the errata (AT400/AT401). I'm sorry i'm not sure i can help much here as I am not familiar with the workaround that was implemented. The ARM errata clearly states that this bug was fixed back in the r2p1 core.
This errata is present in our OMAP35x processor family, which uses an older ARM core.
Regards,
James