My questrion is similar with that in http://e2e.ti.com/support/arm/sitara_arm/f/791/p/302792/1055972.aspx#1055972, but I am still misunderstanding with something.
Chip: AM33359 (Beaglebone Version A6)
OS:Linux 3.2
I am sending data from an FPGA by using the GPMC bus(CS1). My configuration:
[ 1.121124] GPMC_CONFIG1:e8001001 //Burst, sync, 8-bit, non multiplexed, Nor device, FCLK/2
[ 1.124572] GPMC_CONFIG2:00181800
[ 1.128051] GPMC_CONFIG3:22181810
[ 1.131500] GPMC_CONFIG4:18007818
[ 1.134948] GPMC_CONFIG5:000a1818
[ 1.138427] GPMC_CONFIG6:8e060000
[ 1.141876] GPMC_CONFIG7:00000f01 // CS1
gpmc timing setting:
#define GPMC_FPGA_SYNC_CLK_NS (20)
static struct gpmc_timings aplus_fpga_timings = {
/* Minimum clock period for synchronous mode (in picoseconds) */
.sync_clk = 1000 * GPMC_FPGA_SYNC_CLK_NS, /* 10ns */
.cs_on = 0,
.cs_rd_off = 12 * GPMC_FPGA_SYNC_CLK_NS, /* Read deassertion time */
.cs_wr_off = 12 * GPMC_FPGA_SYNC_CLK_NS, /* Write deassertion time */
/* ADV signal timings corresponding to GPMC_CONFIG3 */
.adv_on = 0, /* Assertion time */
.adv_rd_off = 12 * GPMC_FPGA_SYNC_CLK_NS, /* Read deassertion time */
.adv_wr_off = 12 * GPMC_FPGA_SYNC_CLK_NS, /* Write deassertion time */
/* WE signals timings corresponding to GPMC_CONFIG4 */
.we_on = 0 * GPMC_FPGA_SYNC_CLK_NS, /* WE assertion time */
.we_off = 12 * GPMC_FPGA_SYNC_CLK_NS, /* WE deassertion time */
/* OE signals timings corresponding to GPMC_CONFIG4 */
.oe_on = 4 * GPMC_FPGA_SYNC_CLK_NS, /* OE assertion time */
.oe_off = 12 * GPMC_FPGA_SYNC_CLK_NS, /* OE deassertion time */
/* Access time and cycle time timings corresponding to GPMC_CONFIG5 */
.page_burst_access = 1 * GPMC_FPGA_SYNC_CLK_NS, /* Multiple access word delay */
.access = 5 * GPMC_FPGA_SYNC_CLK_NS, /* Start-cycle to first data valid delay */
.rd_cycle = 12 * GPMC_FPGA_SYNC_CLK_NS, /* Total read cycle time */
.wr_cycle = 12 * GPMC_FPGA_SYNC_CLK_NS, /* Total write cycle time */
/* The following are only on OMAP3430 */
.wr_access = 7 * GPMC_FPGA_SYNC_CLK_NS, /* WRACCESSTIME */
.wr_data_mux_bus = 3 * GPMC_FPGA_SYNC_CLK_NS, /* WRDATAONADMUXBUS */
};
I have a 8-bit counter inside the FPGA incrementing with the falling edge of the gpmc_clk.In this way, data are sending to the ARM on the rising edge of the gpmc_clk and they change (from the FPGA side) on the falling edge of the clock.
linux read driver is simple as below:
static void omap_read_buf8(struct omap2_aplus_fpga_dev *fpga_dev, u_char *buf, int len)
{
ioread8_rep((void __iomem *)fpga_dev->virt_base, buf, len);
}
When I read 16 bytes every time from user space programme, it just retured:
... [ 264.266845] aplus_fpga read count 16 [ 264.279724] aplus_fpga read 16, fpga_phys_base 01000000,virt_base d1000000 read buf conrtent: 1 1 11 11 21 21 31 31 41 41 51 51 61 61 71 71 [ 269.292388] aplus_fpga read count 16 [ 269.305419] aplus_fpga read 16, fpga_phys_base 01000000,virt_base d1000000 read buf conrtent: 81 81 91 91 a1 a1 b1 b1 c1 c1 d1 d1 e1 e1 f1 f1 ...
Waves on the oscilloscope in attachments.
wave of each read cycle
Qeustion 1: No matter I set the device width 8 or 16bits, burst or single mode, it just the same result. "8-bit wide devices are supported only in single synchronous or single asynchronous read or write mode"(Please see section 7.1.3.3 in the AM335X TRM Rev.I).It makes me wonder.
Question 2:I can't get "1 2 3 4 5 6 7 8 9 a b c d e f..." as excepted but "1 1 11 11 21 21 31 31 41 41 51 51 61 61 71 71" indeed.It seems that I can only read the first byte and other 7 bytes lost during every read cycle(with 12 gpmc_clk,oe assert on 4th gpmc_clk, 8 bytes output), why? Is my linux driver programme wrong?