This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can AM335x support 1GB DDR3 (512MB*2) when using DDR interface?



Hi team, I have a question on the supporting of 1GB DDR3 (512MB*2) when using DDR interface in AM335x. One of our customers is using MT41K512M16 which has two 512MB banks and two CS signals. In our AM335x’s DDR interface, there is only one CS signal. How could the customer deal with it? Or should the customer use EMIF interface instead? Thanks!