This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM3359: USB project build issue

Part Number: AM3359


Tool/software: TI-RTOS

Hi TI,

                     beaglebone black, processor SDK RTOS 4.2.0.9, ccs 7.4

I am working on usb bulk transfer, and tried to use USBHCDPipeWrite() instead of  USBHCDPipeSchedule(). However this adjustment is hit by error message of "No source available for "do_AngelSWI(int, void *) ". Below attaches my codes,

void USBHCDCSendChars(unsigned char *pucData, uint32_t ulSize, tUSBHCDCInstance *USBHCDCDevice)
{

    USBHCDPipeWrite( USBHCDCDevice->ulIndex,
                     USBHCDCDevice->ulBulkOutPipe,
                     pucData,
                     ulSize);

//    USBHCDPipeSchedule( USBHCDCDevice->ulIndex,
//                        USBHCDCDevice->ulBulkOutPipe,
//                        pucData,
//                        ulSize);
}

I am wondering whether this error actually relates to stack/heap memory size. There is an icf file in IAR system (I am more familiar with) defines

define symbol __ICFEDIT_intvec_start__ = 0xFFFF0000;
 
/*-Memory Regions-*/
define symbol __ICFEDIT_region_ROM_start__ = 0x00000000;
define symbol __ICFEDIT_region_ROM_end__   = 0x00000000;
define symbol __ICFEDIT_region_RAM_start__ = 0x80000000;
define symbol __ICFEDIT_region_RAM_end__   = 0x87FFFFF8;
/*-Sizes-*/
define symbol __ICFEDIT_size_cstack__   = 0x10000;
define symbol __ICFEDIT_size_svcstack__ = 0x1300;
define symbol __ICFEDIT_size_irqstack__ = 0x3000;
define symbol __ICFEDIT_size_fiqstack__ = 0x3000;
define symbol __ICFEDIT_size_undstack__ = 0x1300;
define symbol __ICFEDIT_size_abtstack__ = 0x1300;
define symbol __ICFEDIT_size_heap__     = 0x20000;

my questions come in two-fold,

1. Please advise how to define stack/heap memory in CCS7 for TI_RTOS.

2. is this error specific for my codes, i.e., USBHCDPipeWrite must follow particular procedure.

Please advise, thanks in advance

Mike