This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What is pin assignment of DAC34H84 to display four simple digital signals on oscilloscope?

Other Parts Discussed in Thread: DAC34H84, DAC3482, DAC34SH84, DAC3484

We bought a DAC34H84 for a Stratix IV Altera board. We are going to send only four digital signals to 4 channels of DAC board and see them on the oscilloscope. My question is that as well as four 16-bit signals sent to LVDS negative and positive input data, what would be other signals required for displaying all waveforms via DAC board?? Could you please tell me the type and features of signals that should be send to the suitable pins of DAC board? Or do you have an simple example file with all pin assignments for  all data, clock and control signals to display only four simple digital signals via DAC34H84 ?