This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
I have download two files and then read the memery out .The following are the results of the code memery comparison.Do these differences have an impact on the operation?
Hi!
Unfortunately, you don't provide enough information for me to really understand the differences between the two versions. However, there are a few things that come to mind:
* Pad bytes might not be written to the device, so the content of those bytes may differ.
* When using Debug information for C-SPY, you can replace some modules like __write with others that can talk with C-SPY. Try to uncheck "With runtime control ..." and "With I/O emulation...", to make the two version more alike.
Anyway, I could take a closer look at this. However, I would need a minimal example that demonstrates the problem.
-- Anders Lindgren, IAR Systems, Author of the IAR compiler for MSP430
OK ,thanks,it's useful when I tried to uncheck "With runtime control ..." and "With I/O emulation...".So I want to know What these two options do?
The "With runtime control" checkbox (i.e. the option -r is passed to the linker) replaces some routines like "exit", "abort", and a support routine for "assert" so that C-SPY can notice when these things occur.
The "With I/O emulation" checkbox (i.e. the option -rt is passed to the linker) replaces some additions routines, so that C-SPY can pick up output and input (e.g. plain printf:s and opening files on the host).
-- Anders
**Attention** This is a public forum