This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
We are now promoting our TMCS1126xxA. And we can saw from the datasheet that precision signal conditioning circuitry with built-in drift compensation is capable of less than 1.45% maximum total error over temperature and lifetime with no system level calibration.
Could you please kindly help check how can we calculate this 1.45%?
For example, Sensitivity error: ±0.1%, Non-linearity: ±0.1%, lifetime drift: ±0.5%.
Thanks,
Brian
Hi Brian,
Thanks for the question and using the E2E forum.
We're looking into this and will give you an update when we return from the holiday week.
Louis
Hey Brian,
The 1.45% value is based on maximum sensitivity error (±0.45%), maximum sensitivity thermal drift (±50ppm over 100°C rise max), and sensitivity lifetime drift (±0.5%). So 0.45 + 0.005*100 + 0.5 = 1.45%
Regards,
Mitch