I am having problems connecting to my HVMTRPFC kit to download and debug a project (from the ControlSuite examples)
The thread link below looked very similar, however even after working through it, I still get some variation of the "Error Connecting to Target" message
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/43494.aspx?PageIndex=1
My setup is as follows:
OS: WIndows 7 64 bit
EVK: HVMTRPFCKIT (F28035)
CCv4.2.4.00033 (first install was 4.1.3 but upgraded as part of this process)
M3-J5 no jumper
Connection: Texas Instruments XDS100v1 USB (also tried v2)
Board or Device: Developers Kit - High Voltage Motor Control and PFC (F28035)
Project: HVACI_Sensorless [F2803x_RAM]
Device Manager sees TI XDS100 Channel A and B under USB Controllers
Device Manager sees USB Serial Port COM6
I ran the GUI demo which successfully communicated with the kit using COM6
Different combinations of powering down/disconnecting the EVK and re-starting CCv4
I have tried connecting to the target through the project (Debug Active Project) and non-project debug (Launch TI Debugger | Connect Target)
I always get some form of the "Error Connecting to Target" message.
Error connecting to the target:
(Error -1041 @ 0xFFFFFF87)
The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation.
(Release 5.0.429.0)
Error connecting to the target:
(Error -1135 @ 0x0)
The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation.
(Release 5.0.429.0)
I'm not sure what to try next. Any ideas or suggestions are welcome.
Glen