Hi
Did anybody try this configuration? Does it work?
I've bought this emulator and trying to get it to work in CCS5.1. I've read the wiki topics about xds100, but most of the info is about Windows environment.
I've experienced problems connecting CCS 5.1 to this emulator. I usually get this two types of errors:
----
Error connecting to the target:
(Error -1146 @ 0x0)
Device ID is not recognized or is not supported by driver.
----
and
----
Error connecting to the target:
(Error -1178 @ 0x6D)
Device functional clock appears to be off. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK).
----
I don't even know if the JTAG xds100v2 (by Olimex) was properly recognized by Ubuntu. I haven't installed any drivers as it was said that CCS should have all that is needed. All the info I got from dmesg is as follows:
----
[446851.632967] usb 1-1: new high speed USB device using ehci_hcd and address 4
[446851.782285] usb 1-1: configuration #1 chosen from 1 choice