We use SVN for managing source code changes and are now in the process of integrating this into CCSv5.1. We can download the subclipse plugin and notice it doesn't seem to work with linked files. Our CCS projects contain mostly linked files (e.g. files residing outside the project folder). This files aren't recognized by the plugin. The screenshot below illustrates the problem. Files that are in the project folder show SVN info and can be compared to base versions in the repository. files linked into the project won't do this. Is this a bug? Is there a workaround? Thanks - Mike